Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Product List
The Archer IDC cable-to-board option provides cable connection to 0.635mm pitch flat 30AWG ribbon cables. IDC contacts make connection to the wire by cutting through the insulation as part of the process of wire assembly to the connector. Therefore, no wire stripping is required, making the Archer a fast, single-operation connector.
PTM Published on: 2010-06-14
PTM Updated on: 2017-10-19