Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Product List
One of the main requirements of TVSS overvoltage protection modules is the capability of handling a surge current pulse of 8/20 µs. For this application, EPCOS recommends the ETFV25 series with a surge current capability of 20 kA 8/20 µs. This product can cope with a surge current about 100% greater than that handled by the ETFV20 mm series. EPCOS is one of the few manufacturers worldwide to offer a ThermoFuse varistor with a 25mm disk. Its electrical parameters correspond to those of the 25mm disk varistor.
PTM Published on: 2011-10-27