Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
X2Film-Slide14
In summary, the heavy duty B3293x series from EPCOS offers a new range of AC film capacitors with capacitance values from 0.047µF to 10µF, and rated at 305 VAC at 105°C. EPCOS has achieved in one product extremely high capacitance stability under hard environment conditions, within small dimensions and featuring the safety certifications of an X2 capacitor. This series fits perfectly with the new requirements of the market and, in summary, offers the following advantages: it is suitable for high humidity environments, has high capacitance stability under harsh conditions, there is no need to oversize the components in the circuit, it enables significantly reduced volume compared to other reliable solutions, and most importantly it is approved according to the basic standards for capacitors, IEC60384-14 and UL60384-14.
PTM Published on: 2010-11-16