Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
setup

The next step is to insert the SD Micro Card, connect the keyboard, mouse, HDMI from the monitor, and the Ethernet cable. After everything is connected the user can connect the power supply to the Raspberry Pi. The screen will scroll through Linux type code as the Raspberry Pi boots up and will come to a desktop like the one shown in the image on this slide.