Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
mounting hard drives

When the NTFS command has downloaded and installed, users will need to know the name of each of the hard drives. This is done with typing the command: sudo fdisk-L and then press enter. The names are listed here in the lower left example are: one is the SDcard that the operating system is on. Second is the same drive with no information and can be listed as sda1 if there is information on the drive. Finally, the third one is a separate drive.