Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Product List
The PMP series has many features that benefit the user, ranging from its size to its selectability of operation modes. Most importantly is the selectable operation mode which allows the user to select between Phase Angle or Burst Fire modes, and within each of those the control range is selectable. This gives the user a large range of freedom to choose which mode best suits the application. The PMP comes with built-in internal over-temperature protection, which will turn off the unit if the internal temperature exceeds 80°C, preventing damage to the PMP. From a size perspective, the PMP features a compact 22.5mm panel mount housing allowing it to get into tight areas. It comes with “Elevator Screw” output terminations that allow for use of bare wire, fork, and ring terminations. Lastly, input connections to the PMP use a removable input connector that allows the control wiring to be attached separately and then plugged into the PMP. Great for using pre-fabricated wire harnesses.
PTM Published on: 2017-11-30