Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Product List
Additionally, Bourns power resistors have good solderability with a nickel barrier and either gold or tin. The use of gold removes the need for tin whiskers. A stable VSWR over the entire frequency range is important for RF performance. Bourns also conforms to the industry standard with regard to mechanical size and main features of power, materials, and frequency.
PTM Published on: 2011-10-19