Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
SmartMeter-Slide9

AVX offers ready made solutions for each of the applications shown on this page. For power hold-up, especially for remote, battery operated systems, or systems that must maintain operation during power glitches, the BestCap pulse supercapacitor is ideal. For all DC-DC and AC-DC power filtering, low ESR tantalum chip capacitors, in the 100uF / 10v range will handle the majority of Smart Meter applications. Depending on ripple, TPM multi-anode tantalum for ultra-low ESR is ideal, while Hi CV MLCC can be used for the input side.  Digital / Analog conversion in both directions is relying on new generation DSPs which can handle faster data rates. These devices need decoupling capacitors with low inductance such as the LICC, IDC & LGA ceramics to preserve signal integrity. Touchscreens and LCD displays need ESD protection and filtering of the RGB display lines from RF interference. AVX offers circuit protection products such as Transguard for ESD and Feedthru for filtering. These can also be used for antenna protection, especially the antenna guard and sub-picofarad varistor (SPV) products. The RF block and Home Area Network benefit from AVXs wide range of high-frequency / Microwave products – From Low ESR “U” dielectric to high precision thin film RF capacitors and couplers in matching circuits. Similarly, there is a whole suite of TCXO, crystals, and oscillators tailored to every wireless protocol. While these devices all form the “passive glue” to hold the blocks together electrically, physical interconnection is also a necessity such as the  FFC , FPC and  BTB interconnect systems.

PTM Published on: 2011-09-06