Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
FAKRA-Slide4

In the FAKRA product series, there are 14 housing colors which pertain to the mechanical rib combinations. The plastic housings are designed with visually and mechanically coded and keyed tooling to eliminate assembly errors. The housing is designed to make an audible clicking noise when mated and it also features a locking mechanism to ensure a solid connection. Our connector can be used with a multitude of coaxial cables and numerous configurations such as right angle, edge launch and PCB mount designs.

PTM Published on: 2011-10-24