After the execution of a command (busy=0) the expected data can be read as illustrated in Figure 3, or if no data is returned by the command the next command can be sent. All mandatory I2C- bus protocol features are implemented. Optional features like clock stretching and 10-bit slave address, are not supported by the sensor’s interface.