Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Product List
In summary, ATS’ re-circulating and immersion chiller series are easy-to-use, portable systems. Because of their vapor compression based refrigeration ATS chillers are for cooling only, they do not provide any heating of the coolant. In the ATS re-circulating chillers the temperature of the chilled fluid can be easily set from the front panel which also shows the pressure drop between the inlet and the outlet. ATS’ chillers have a fast response time because of the precise PID control system, with small temperature fluctuations. ATS’ immersion chillers require no additional plumbing from the chiller to the tank. The thermal transport between the fluid tank and the chiller takes place via the ATS iM evaporator which is connected to the refrigeration system via a 1.6 m long hose. ATS chillers are ideal for laboratory testing, industrial processing, sensor calibration, bio-medical testing, laser thermal management, component characterization, and other industrial applications.
PTM Published on: 2016-09-19