Getting Started with STM32 and Nucleo Part 1-Introduction to STM32CubeIDE and Blinky
2019-08-27 | By Maker.io Staff
In this video, Shawn Hymel introduces the ST Microelectronics STM32CubeIDE (Integrated Development Environment) for 32-bit development boards with the STM32 chip. Using the Nucleo-F042KS development board as an example, Shawn steps through the setup process, coding examples and explains some of the more advanced aspects of STM32CubeIDE such as the line-by-line debugging features. Useful tips on browsing the helpful ST documentation are also discussed.
Related Items
Related Project
Related Videos
Recommended Reading
- Getting Started with STM32 and Nucleo Part 2: How to Use I2C to Read Temperature Sensor TMP102
- Getting Started with STM32 and Nucleo Part 3: How to Run Multiple Threads with CMSIS-RTOS Interface
- Getting Started With STM32 & Nucleo Part 4: Working with ADC and DMA
- Getting Started with STM32 - How to Use SPI
- Getting Started with STM32 - Timers and Timer Interrupts
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.
Visit TechForum