Maker.io main logo

SparkFun Thing Plus Matter - MGM240P Hookup Guide

76

2024-02-27 | By SparkFun Electronics

License: See Original Project Wireless

Courtesy of SparkFun

Guide by EL DUDERINO

Introduction

The SparkFun Thing Plus Matter - MGM240P is the first easily accessible board of its kind that ‎combines Matter® and SparkFun's Qwiic ecosystem for agile development and prototyping of ‎Matter-based IoT devices. The board features the MGM240P wireless module from Silicon Labs®. ‎The MGM240P provides secure connectivity for both 802.15.4 (Matter, Zigbee®, and OpenThread®) ‎and Bluetooth Low Energy 5.3 protocols and is built to integrate seamlessly into the Matter IoT ‎protocol using the Simplicity Studio IDE from Silicon Labs.‎

SparkFun Thing Plus Matter - MGM240P

 

 

You may be curious as to what exactly Matter is. In a nutshell, Matter allows for consistent operation ‎between smart home devices and IoT platforms without an Internet connection, even from different ‎providers. This allows communication between major IoT ecosystems to create a single wireless ‎protocol that is easy, reliable, and secure to use.‎

This guide covers the hardware present on this Thing Plus development board, basic assembly, ‎and a quick intro to using the Thing Plus Matter in Silicon Labs' Simplicity Studio development ‎environment.‎

Required Materials

All you need to follow along with this tutorial is the SparkFun Thing Plus MGM240P as well as a ‎USB-C cable to connect it to your computer for programming. You may also want a single-cell LiPo ‎battery to power the board in your application.‎

Optional Accessories

Depending on your application's needs, you may want some additional accessories along with the ‎Thing Plus Matter - MGM240P and USB-C cable.‎

LiPo Battery

The Thing Plus Matter includes a 2-pin JST connector to connect a single-cell lithium-ion battery for ‎power in mobile applications. Below are a few options we recommend:‎

Headers

Headers allow you connect external parts to your board with just a set of jumper wires for ‎prototyping circuits with a breadboard. The list below outlines a few options we recommend. If you ‎don't find what you need, check out our Headers Category. If you need soldering tools, head over ‎to our Soldering Category:‎

Solder Jumper Modification

The Thing Plus Matter - MGM240P has several solder jumpers users can modify to change ‎behavior on the board. Modifying the jumpers requires a knife and soldering equipment. The list ‎below covers some recommended options but in case you do not find what you need there, head ‎over to our Soldering Category:‎

Suggested Reading

Before getting started with this Hookup Guide, you may want to read through the tutorials below if ‎you are not familiar with the concepts covered in them or want a refresher:‎

  • How to Solder: Through-Hole Soldering: This tutorial covers everything you need to know ‎about through-hole soldering.‎

  • Serial Communication: Asynchronous serial communication concepts: packets, signal levels, ‎baud rates, UARTs and more!‎

  • Serial Peripheral Interface (SPI): SPI is commonly used to connect microcontrollers to ‎peripherals such as sensors, shift registers, and SD cards.‎

  • Logic Levels: Learn the difference between 3.3V and 5V devices and logic levels.‎

  • I2C: An introduction to I2C, one of the main embedded communications protocols in use today.‎

  • Analog vs. Digital: This tutorial covers the concept of analog and digital signals, as they relate to ‎electronics.‎

  • Bluetooth Basics: An overview of the Bluetooth wireless technology.‎

  • How to Work with Jumper Pads and PCB Traces: Handling PCB jumper pads and traces is an ‎essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to reroute ‎connections, and repair a trace with the green wire method if a trace is damaged.‎

Hardware Overview

In this section we'll take a closer look at the MGM240P as well as other hardware present on the ‎Thing Plus Matter - MGM240P.‎

MGM240P

The MGM240P wireless module provides a secure solution for both 802.15.4 (Matter, Zigbee, and ‎OpenThread) and Bluetooth Low Energy 5.3 protocols, and is designed to integrate seamlessly into ‎the Matter IoT convention. Matter aims to simplify and consolidate major Smart Home IoT ‎ecosystems into a single, secure, and easy to use protocol.‎

module_1

The MGM240P is built around Silicon Labs' EFR32MG24 wireless system-on-chip (SoC) that ‎includes a 32-bit ARM Cortex M33 core processor and integrated 2.4 GHz radio, 1536 kB Flash ‎memory, and 256 kB of RAM. The Thing Plus runs the MGM240P at 3.3V by default when powered ‎by USB or a battery. The module has a dedicated processor core for security to allow for use with ‎Silicon Labs' Secure Vault IoT security feature suite along with a host of software-configurable ‎options using the Simplicity Studio IDE. This Thing Plus specifically uses the MGM240PB32VNA ‎variant of the module which uses a built-in antenna with a max transmit power of +20 dBm. For a ‎complete overview of the MGM240P refer to the datasheet.‎

J-Link Debugger

The board uses the EFM32GG12B410F1024GL120-A microcontroller as a J-Link programmer and ‎debugging IC. The Mini Simplicity Connector on the board allows users to connect an external ‎debugger if they wish. The board pulls the debugger WAKE pin to V_USB through the LP jumper ‎by default to have it operate in standard mode. Users can open this jumper to force the debugger ‎into Low Power mode.‎

The debugger allows some seriously low-level debugging tools when used with Simplicity Studio's ‎debugging tool. You can perform all sorts of standard debugging actions such as debugger output, ‎placing code breaks, and can even get as granular as looking at the assembly code.‎

Power

The Thing Plus Matter - MGM240P offers several ways to power the board. The primary power ‎options are the USB-C connector (also used for programming/serial communication) and 2-pin JST ‎connector for a single-sell LiPo battery. The board includes the necessary components to charge ‎and monitor the charge level of a connected battery.‎

power_2

The board also has PTH pins connected to the 3.3V, V_USB, and V_BATT nets.‎

USB-C

The USB-C connector on the board provides power, battery charging voltage, and a serial ‎connection for programming and interfacing. The board also includes a USB shield jumper that ‎controls whether or not the USB shield pin on an attached cable connects to the board's ground ‎plane.‎

The 5V from V_USB connects to the 3.3V regulator as well as the VIN on the LiPo battery charger ‎so the MCP73831 is powered with voltage present from USB so long as the CHG solder jumper is ‎set to either current setting. Opening the jumper disables the MCP73831.‎

LiPo Connector and Charge Circuit

The board includes a 2-pin JST connector to plug a single-cell LiPo battery in for battery powered ‎applications. The input voltage is regulated by a 3.3V voltage regulator. The board also features a ‎MCP73831 Single-Cell LiPo Charge IC to recharge a connected battery when plugged in over USB-‎C as well as a MAX17048 Single-Cell fuel gauge to monitor battery charge level.‎

By default, the charge current is set to 500mA. A three-way jumper labeled CHG allows users to ‎switch between 500mA charge current to 100mA as well as disabling the charge IC when not ‎needed. More on this and all other solder jumpers in the Solder Jumpers section below.‎

Pinout

The MGM240P has 26 General Purpose Input/Output (GPIO) pins that are all individually ‎configurable through software to act as I/O pins, peripherals (SPI, I2C, etc.) or other advanced ‎configurations such as open drain. This allows remapping of any GPIO to any supported ‎functionality.‎

pinout_3

The Thing Plus Matter - MGM240P breaks out 23 of these pins to PTHs on either side of the board. ‎The board settings configures them to deliver the following functionality:‎

  • Serial - TX/RX

  • I2C - SDA/SCL

  • SPI - POCI/PICO/SCK

  • Analog - A0-A5*‎

  • GPIO - 0-6*

  • Freebie - Feather-compatible Freebie pin tied to PC07

  • Reset

  • Enable

Note: Despite their labels, all GPIO pins (A0-A5 and GPIO0-GPIO6) function as either GPIO or ‎analog.

‎Peripheral Accessories

The Thing Plus MGM240P includes several peripheral accessories that allow users quick access to ‎several features. Let's take a brief look at them.‎

peripheral_4

Mini Simplicity Connector

The Mini Simplicity Connector allows users a quick and direct option to connect an external ‎debugger to the board.‎

Note: An external Mini Simplicity debugger plugged into the board connects to the serial (TX/RX) ‎pins of the on-board debugger IC meaning only one debugger is available at a time (either external ‎or on-board.)

‎‎µSD Slot

The µSD card slot provides an option to connect a µSD card for extra memory space to the Thing ‎Plus.‎

Qwiic Connector

The Qwiic connector provides a fast connection to the I2C bus to use with SparkFun's ever-‎growing Qwiic ecosystem.‎

LEDs

This board has four LEDs labeled PWR, STAT, CHG, and DBG.‎

leds_5

  • Power (PWR) LED - Indicates power supplied to the board.‎

  • Status (STAT) LED - Tied to A8 for use as a general status indicator.‎

  • Charge (CHG) LED - Indicates whether or not the charge circuit is actively charging an ‎attached LiPo battery.‎

  • Debugger (DBG) LED - Connects to the debugger IC's status output and can provide visual ‎indication for debug behavior.‎

Solder Jumpers

If you have never worked with solder jumpers and PCB traces before or would like a quick ‎refresher, check out our How to Work With Solder Jumpers and PCB Traces tutorial for detailed ‎instructions and tips.‎

The board has nine solder jumpers for user customization. The table below outlines the jumper's ‎label, default state, function, and any notes regarding how to use them.‎

solder_6

table_7

digital multimeter

Board Dimensions

The Thing Plus - MGM240P matches the Thing Plus footprint to work with all Thing Plus-compatible ‎accessories and shields and measures 2.30" x 0.90" (58.42mm x 22.86mm). The two mounting ‎holes on this Thing Plus fit a 4-40 screw.‎

dimensions_8

Hardware Assembly

Now that we're familiar with the hardware on this Thing Plus it's time to assemble the board into a ‎prototyping circuit or simply plug it into our computer with a USB-C cable and get right to ‎programming.‎

Basic Assembly

For those who want to jump right in to using the Thing Plus Matter - MGM240P on its own or just ‎with the wireless capabilities, all you need to do is plug the board into your computer using a USB-C ‎cable.‎

basic_9

Soldering Headers

Users who want to assemble a prototyping circuit with the Thing Plus should solder headers of their ‎choice to the board to plug it into a breadboard. We recommend something like this Feather ‎Stackable Header Kit.‎

Software Setup

The MGM240P uses Silicon Labs' Simplicity Studio IDE as a development tool for programming, ‎debugging, customizing, etc. In this section we'll cover the basics of installing the IDE and adding ‎the Thing Plus Matter.‎

Install and Open Simplicity Studio

Simplicity Studio is available for Windows, Mac OSX and Ubuntu operating systems. You can find ‎the installer download for your operating system by clicking the button below:‎

SIMPLICITY STUDIO DOWNLOADS

Silicon Labs requires you to create a (free) account to download Simplicity Studio so make one if ‎you do not have one already. Once the installer finishes downloading, open it and follow the ‎installation instructions.‎

Simplicity Studio Launcher

When you first open Simplicity Studio, you'll be greeted by the Launcher window. The default ‎Launcher window lets users install board files for both connected devices and by searching for a ‎supported product. It also lists any recent projects you've worked on as well as links to user guides ‎and support documentation.‎

documentation_10

On the left side there are two windows for any debug adapters (top) and all installed products ‎‎(bottom). In the very top right of the screen, you'll see the tabs to switch between the launcher, the ‎Simplicity IDE and the Debug window. We'll be using the IDE tab in the next section once we finish ‎installing the Thing Plus Matter into Simplicity Studio.‎

Adding the Thing Plus Matter - MGM240P

Simplicity Studio makes adding devices extremely easy by just connecting the device to your ‎computer over USB and then selecting "Connected Devices". It automatically checks the device ‎ID to matching supported products and should display either as a J-Link Silicon Labs debugger ‎‎(prior to install) or "SparkFun Thing Plus MGM240P" as the connected device.‎

adding_11

With the connected Thing Plus selected, click "Start". This opens the Installation Manager window ‎where you can select either "Auto" or "Advanced" installation. Most users should ‎select "Auto" and then click "Next". You'll be prompted to agree to licensing agreements. Once ‎you have agreed, click "Finish" and it will install all necessary software, drivers, and other ‎packages to use the Thing Plus Matter in Simplicity Studio.‎

install_12

The install process can take a few minutes and once it completes, you'll need to restart the program. ‎After restarting, your Launcher window should update and look similar to the screenshot below:‎

install_13

This window contains several tabs that cover the general overview of the board, examples, ‎documentation and compatible tools. Feel free to explore as much as you'd like but for now, we'll ‎move on to a basic "Blink" example to make sure everything was set up correctly and the Thing Plus ‎Matter is working.‎

Silicon Labs Documentation

For comprehensive information on using Simplicity Studio, Silicon Labs has an in-depth user guide ‎for the IDE available here:‎

SIMPLICITY STUDIO USERS GUIDE

If you're itching to integrate your Thing Plus with a Matter-compatible device, Silicon Labs has ‎documentation for Matter development here:‎

SILICON LABS MATTER DOCS

They also have much more documentation covering other applications including Thread, other ‎wireless protocols, and the Gecko SDK used in Simplicity Studio available on their main ‎documentation page here:‎

SILICON LABS DOCUMENTATION

Blink Example

Now that the Thing Plus Matter - MGM240P is installed in Simplicity Studio we can move on to a ‎basic test to make sure everything is working as intended. For this example, we'll be setting up and ‎uploading a Blink test to turn the Status LED on and off.‎

Blink Example

In the Launcher with the SparkFun Thing Plus MGM240P selected for your product, navigate to ‎the "Example Projects & Demos" tab. Now type "Blink" into the "Filter on keywords" search bar ‎and select "Platform - Blink Bare-metal" and click "Create".‎

blink_14

This opens the New Project Wizard window where you can change the project name, filepath, and ‎project file options. For now, leave all of that with the default settings and click "Finish".‎

project_15

Once you've created the new project you can double-click on the containing folder in the "Project ‎Explorer" window to open all the files included with the Blink project which includes any binaries, ‎configs, header, and C files if you prefer. For now, we're just going to build and flash the project to ‎get the Status LED blinking. To do that, right click on the "blink_baremetal" folder and scroll down ‎to "Run As" and select "1 Silicon Labs ARM Program". This builds and flashes the project to ‎your board and once it completes the Blue STAT LED should be blinking on and off every second.‎

files_16

This is obviously one of the most basic projects for the Thing Plus Matter so from here you can ‎explore other example projects and demos for the Thing Plus or start building your own.‎

Troubleshooting

Power Consumption Tips

Power consumption by this board varies depending on how it is configured and powered. Below are ‎our current consumption test results for various power options with the MGM240P operating in Low ‎Power mode:‎

  • Regulated 3.3V input on 3V3 pin - 15µA

  • LiPo JST Connector/VBAT pin - 120µA

  • USB-C/VUSB pin (LP and CHG jumpers cut) - 250µA

  • USB-C/VUSB pin (only LP jumper cut) - 300µA

  • USB-C/VUSB pin (neither jumper cut) - 21mA‎

As you can see, for lowest current consumption, powering the board with a regulated 3.3V input ‎directly to the 3.3V pin draws significantly less current as it bypasses the voltage regulator and ‎battery charge/monitoring components. All of these tests were performed with the PWR jumper ‎OPEN to disable the Power LED.‎

Driver Installation

Most operating systems will not recognize the Thing Plus Matter as a USB device by default. To ‎install drivers, download and install the Simplicity Studio IDE and then install the Thing Plus Matter ‎package to the IDE. This process will install all necessary board packages for the Thing Plus ‎including USB drivers. Refer to our Getting Started with Simplicity Studio guide or Silicon ‎Labs' Simplicity Studio documentation for detailed instructions.‎

General Troubleshooting

Not working as expected and need help?

If you need technical assistance and more information on a product that is not working as you ‎expected, we recommend heading on over to the SparkFun Technical Assistance page for some ‎initial troubleshooting.

SPARKFUN TECHNICAL ASSISTANCE PAGE‎

If you don't find what you need there, the SparkFun Forums are a great place to find and ask for ‎help. If this is your first visit, you'll need to create a Forum Account to search product forums and ‎post questions.

CREATE NEW FORUM ACCOUNT     LOG INTO SPARKFUN FORUMS

Resources and Going Further

That's all for this guide. For more information about the SparkFun Thing Plus Matter - MGM240P, ‎check out the following resources:‎

SparkFun Thing Plus Matter - MGM240P Resources

Silicon Labs Resources

Looking to use the Thing Plus Matter - MGM240P with the Matter platform? Check out this tutorial on how to set up the Thing Plus with a Google Nest Hub™:

thing_18

Connecting Thing Plus Matter to Google Nest Hub

Connect your Thing Plus Matter board to a Google Nest Hub, as well as the Google Home app, and set up as a light device!

制造商零件编号 20270
THING PLUS MATTER MGM240P
SparkFun Electronics
制造商零件编号 15426
CBL USB2.0 A PLUG TO C PLG 0.98'
SparkFun Electronics
制造商零件编号 14743
CABLE A PLUG TO C PLUG 3.28'
SparkFun Electronics
制造商零件编号 15424
CBL USB2.0 A PLUG TO C PLG 6.56'
SparkFun Electronics
制造商零件编号 00116
BREAK AWAY HEAD
SparkFun Electronics
制造商零件编号 14681
SPARKFUN BEGINNER TOOL KIT
SparkFun Electronics
制造商零件编号 09200
HOBBY KNIFE
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.