制造商零件编号 A000005
ARDUINO NANO ATMEGA328 EVAL BRD
Arduino
License: See Original Project Arduino
Courtesy of All About Circuits
Make your own sous-vide machine with an Arduino and a rice cooker. This project can be built in a weekend and is easy to maintain. Sous-vide machines are mostly used for meat, vegetarians can also make use of this device.
What Is a Sous-Vide Machine?
The name is a little misleading even if you speak French. "Sous vide" means "under vacuum" in French.
Traditionally, step one is to place the food to be cooked into a plastic bag and vacuum it closed. You then lower the bag into the machine, which is filled with water heated to a precise temperature. (As a note, you don't necessarily need to fully vacuum pack the food. You can just as easily put the food into an open bag and lower its bottom half into the machine, allowing the pressure of the water to remove the air around the food.)
This is a culinary method developed to essentially boil foods, especially meats, without losing juices or flavor into the water. But what's the benefit? Wouldn't it be better (and easier) just to cook a steak in a skillet?
Let’s presume that you enjoy your steak medium rare. When you cook it in a pan, the meat isn’t uniformly cooked because it is cooked from the outside in. This results in the middle being perfectly cooked and pink, but then moving farther away from the center it is more medium, and it might even be well done on the outside.
If we cook that same steak in a sous-vide machine, the piece of meat would be cooked evenly all the way through. Here is a picture to better understand what is happening:
BOM
We’ll be using a rice cooker in order to make our sous-vide machine as simple as possible. The heater and water container are housed in the rice cooker. Without further ado, here is the complete BOM:
*You could use a DS18B20 instead but you'd need to change the code accordingly*
The Hardware
Let’s now talk about the hardware aspect of this project. Here is the schematic:
Please connect everything as you see in the schematic. Below I will try to explain why we chose the specific components and how they work.
MCU (Microcontroller Unit)
For the “brains” of this device, we will be using a very basic development board: the Arduino Nano. It has the same microcontroller, ATMEGA328, as the Arduino Uno, but in SMD form.
LCD
The LCD is a common 16×2 character display with a Hitachi HD44780 controller. Attached to it is an I2C board that also contains a potentiometer for contrast adjustment. I used this because we will only need four pins to communicate with our Arduino: two for power and two for data.
Relay
The LEG-5 relay is a through-hole component that acts as a switch, closing when current is driven through the coil. You can use any other relay; just make sure that the nominal coil voltage is 5 V and that it has an inductive AC contact rating at least 1.5 times greater than the current required by your rice cooker. For example, my rice cooker needs about 2 A AC, and the LEG-5 relay has a rating of 3 A.
In the schematic, you’ll notice that there’s a diode in parallel (actually, strictly speaking, it is antiparallel) with the relay coil. This diode is called (among other names) a flyback diode, and it protects the transistor by providing a path for the inductive current that continues to flow after the transistor is turned off.
Another important aspect of this project is how to “tap into" the extension cord. (We're using an extension cord because we don't want to ruin the cord attached to the rice cooker.) We need to create a break in one of the extension cord wires and insert our relay.
Household electrical cables consist of “line”, “neutral”, and “ground”. In order to properly turn on or off the sous-vide machine, we need to insert a relay in the line conductor. We could put the relay in the neutral conductor, but it is good practice to use the line conductor because this approach can provide extra protection against electric shock. You can determine which wire is the line with a mains tester or by following the specific wiring color codes for your country. You can find more about color codes here. Another good practice is to use a double relay or two relays to switch both the line and the neutral.
Important note: When building this project, be careful with the mains voltage. Always make sure everything is unplugged when you are tinkering with the wires, and arrange the wiring such that it is impossible for the (exposed) line and neutral conductors to come into contact. If you aren’t 100% sure about what you are doing, please ask in the comments or in the forum before you continue with your project.
Continuing with the switching part of the schematic, you can see that there is an NPN transistor and a resistor there. This is to amplify the current needed to energize the coil of the relay. We need this because the current needed by the relay (72 mA) is greater than what our microcontroller can output (the absolute maximum I/O-pin output current is 40 mA, and typical operating currents should be significantly lower). The resistor is needed to limit the current going into the base of the transistor, which is intended to operate as a switch (i.e., in the saturation region). You can read more about this subject here and here.
Buttons
The switches are normal pushbutton switches that are closed only when they are pressed (they do not maintain that state after release). We do not need any external pull-up resistors because we will be using the microcontroller's internal pull-ups. You can find more information on switch types here.
Temperature Sensor
The backbone of this project is the temperature sensor, the MCP9701. I didn’t choose this particular device for any specific design reasons; it was just what I had available. It has decent accuracy, and the interface is straightforward - it outputs a voltage (VOUT) proportional to the ambient temperature (TA), with a slope (TC, i.e., Temperature Coefficient) of 19.5 mV/°C and an offset voltage (V0°C) of 400 mV.
When you place the sensor in the sous-vide, I recommend putting it in the center of the pot, or at least close to the plastic bag that contains the to-be-cooked item.
Since this temperature sensor isn’t waterproof, we’ll need to solder wires to it and then dip it in epoxy so that any conductive part is covered. Here is how mine turned out:
My waterproofed temperature sensor
If you’d like to spare yourself the trouble of waterproofing your sensor, you can use an already waterproofed sensor.
On the schematic, there is a decoupling capacitor, C1. My circuit worked well without it, but it's a good idea to include it.
Power Supply
Finally, the power supply! One 5 V supply is used for the entire circuit. You should find something that can source at least 150 mA. For example, a mobile phone charger will do the job.
Software
Now that we are done with the hardware, let’s look at the software.
You can see that there are two files: "main.ino" and "main.h". The header file, with the extension ".h", includes declarations for all the variables and constants used and also the "include" directives, because we are using two libraries, which you will need to install. The first library used is the PID library by Brett Beauregard. This controls the relay to obtain the desired temperature, and the second one is a library for controlling the LCD via I2C. If you wish to change parameters or what pins to use, you should do this in the header file.
The "main.ino" file contains the basic Arduino functions "setup()" and "loop()". In setup() we initialize all the variables that need a default value and also set the pins as either output (for the relay) or input (for the switches).
In the main loop we call five functions:
double realtemp = ((average * (5000.0 / 1023.0)) - 400) / 19.5;
Conclusion
That’s it, guys! If you have followed the instructions step-by-step, go and prep your meal now because the sous-vide machine is ready for action, and I'm sure that you are hungry.
Turn it on, enter the menu, set the temperature, set the cooking time, press start, and enjoy! Here is my try at a sous-vide burger:
If you have any questions or ideas for improving the project, please don’t hesitate to leave a comment. I will try to maintain the project on this GitHub page if you want the latest version of the software, but I cannot guarantee that the information you find here will still be 100% accurate. If you don't need extra features, use the code included on All About Circuits.
What I didn’t mention (because I wanted to keep this project as simple as possible) is a water pump. Professional sous-vide machines have water pumps to circulate the water in order to maintain a uniform temperature. A pump is not necessary, but if you have one available, you might want to try it and see if the results are noticeably improved. You can use an Arduino output pin in conjunction with a transistor to turn it on.
Here is a link to a web page that gives the best temperatures for different types of meat. If you’re looking for sous-vide meal ideas, I recommend browsing Youtube.