制造商零件编号 3000
CIRC PLAYGROUND CLASS ATMEGA32U4
Adafruit Industries LLC
License: See Original Project
Courtesy of Adafruit
Guide by Carter Nelson
This is a fun and simple beginner project that uses the Circuit Playground to create a light activated alarm. A diary, or other object, can be placed on top of the Circuit Playground and an alarm will sound when the object is removed.
Required Parts
This project uses the sensors already included on the Circuit Playground. The only additional items needed are batteries for power and a holder for the batteries.
Before Starting
If you are new to the Circuit Playground, you may want to first read these overview guides.
This project will use the Arduino IDE. Make sure you have added the board support for the Circuit Playground as well as installed the Circuit Playground library. MUST DO BOTH. This is covered in the guides linked above.
Hello Light Sensor
To get an idea of how the alarm works, let's start by exploring the light sensor itself. You can read some technical details in the Lesson #0 Guide. And for reference, here is where the light sensor is located on the Circuit Playground.
There is an example sketch included with the Circuit Playground library that we can use to play around with the light sensor. It can be found in the following location:
File -> Examples -> Adafruit Circuit Playground -> Hello_CircuitPlayground -> Hello_LightSensor
With this sketch loaded and running on the Circuit Playground, open the Serial Monitor.
Tools -> Serial Monitor
The current value from the light sensor will be printed once a second.
Play around with shining different lights on the light sensor and changing the distance. Also try covering the sensor with your hand, a sheet of paper, or anything else lying around (like a diary). The value can range from 0 to 1023, with higher numbers meaning more light is getting to the sensor. When you cover the light sensor, you should see the value go down.
Another way to watch the value of the light sensor is to use the Serial Plotter. To do this, let's first modify the code slightly. The code below removes the text from the output and increases the rate at which the value is displayed.
#include <Adafruit_CircuitPlayground.h>
#include <Wire.h>
#include <SPI.h>
int value;
void setup() {
Serial.begin(9600);
CircuitPlayground.begin();
}
void loop() {
value = CircuitPlayground.lightSensor();
Serial.println(value);
delay(100);
}
With this sketch loaded and running on the Circuit Playground, open the Serial Plotter.
Tools -> Serial Plotter
The light sensor value will now be plotted like a strip chart as shown below. Again, play around with different lighting conditions and watch the value change.
Now we can explain how the alarm is going to work. With a diary placed on top of the Circuit Playground, the light sensor will have a low reading. If the diary is removed, more light will get to the sensor and the reading will increase. An example of what this would look like is shown below.
So if we simply monitor the value of the light sensor and watch for this increase, we can detect when the diary has been removed and sound an alarm.
Alarm Code:
The alarm code works as follows:
Here is the full code listing. You can copy and paste it into the Arduino IDE.
// Circuit Playground Dear Diary Alarm
//
// Don't let sister/brother read your secrets! Place the "armed" Circuit
// Playground under your diary. If someone tries to remove the diary, an alarm
// will sound.
//
// Author: Carter Nelson
// MIT License (https://opensource.org/licenses/MIT)
#include <Adafruit_CircuitPlayground.h>
#include <Wire.h>
#include <SPI.h>
uint16_t lightValue; // current light sensor reading
uint16_t coveredValue; // the light sensor value with diary on top
uint16_t alarmThreshold = 20; // adjust to change alarm sensitivty
bool triggered = false; // becomes true when diary removed
///////////////////////////////////////////////////////////////////////////////
void setup()
{
// Initialize Circuit Playground library.
CircuitPlayground.begin();
// Turn on all the NeoPixels.
for (int p=0; p<10; p=p 1) {
CircuitPlayground.setPixelColor(p, 255, 0, 0);
}
// Wait for button press.
while ( (CircuitPlayground.leftButton() == false) &&
(CircuitPlayground.rightButton() == false) ) {
// Do nothing.
}
// Countdown timer.
for (int p=0; p<10; p=p 1) {
CircuitPlayground.setPixelColor(p, 0, 0, 0);
delay(500);
}
// Compute covered light sensor value as average of 5 readings.
coveredValue = 0;
for (int i=0; i<5; i=i 1) {
lightValue = CircuitPlayground.lightSensor();
coveredValue = coveredValue lightValue;
}
coveredValue = coveredValue / 5;
// Beep to indicate ARMED.
CircuitPlayground.playTone(1000, 1000);
delay(1000);
}
///////////////////////////////////////////////////////////////////////////////
void loop()
{
// Check to see if alarm has been triggered.
if (triggered) {
// Sound the alarm.
CircuitPlayground.playTone(2000, 500);
delay(500);
CircuitPlayground.playTone(3000, 500);
delay(500);
} else {
// Get current light sensor value.
lightValue = CircuitPlayground.lightSensor();
// Check light sensor value to determine if alarm should be triggered.
if (lightValue > coveredValue alarmThreshold) {
triggered = true; // Trigger the alarm.
}
}
}
Using the Alarm
Once the sketch has been loaded on the Circuit Playground, it is ready for use. Install the batteries, plug in the power cable, and turn the switch on. You should see all of the NeoPixels come on and turn red.
All the lights are on. Ready to use.
Press either button to start the countdown timer.
The NeoPixels will turn off one at a time.
BEFORE ALL THE LIGHTS GO OUT, PLACE THE DIARY ON THE CIRCUIT PLAYGROUND.
Make sure the diary covers the light sensor before the countdown ends
When the countdown ends a short BEEP will sound.
If you now remove the diary from the Circuit Playground, the alarm should sound. You can press the RESET button to stop the alarm and start again. Yes, this is an easy way to defeat the alarm, but hopefully you will hear the alarm before someone figures that out.
Questions and Code Challenges
The following are some questions related to this project along with some suggested code challenges. The idea is to provoke thought, test your understanding, and get you coding!
While the alarm sketch provided works, there is room for improvement and additional features. Have fun playing with the provided code to see what you can do with it.
Questions
Code Challenges