制造商零件编号 3000
CIRC PLAYGROUND CLASS ATMEGA32U4
Adafruit Industries LLC
License: See Original Project Wearables Circuit Playground
Courtesy of Adafruit
Guide by Carter Nelson
Overview
In this guide we will use the Circuit Playground to create a bike turn signal indicator. By sewing the Circuit Playground to a bike glove and using the accelerometer to detect hand position the standard hand turn signals are enhanced with some nice NeoPixel animations.
Required Parts
In addition to a Circuit Playground, you will need some form of battery power. The 500mAh battery is a nice low profile option and is recommended for this build. However, you may be able to also use the AAA battery pack if you can incorporate it into your bike gloves. Oh yeah, you'll also need bike gloves and some needle and thread to sew everything together.
Lithium Ion Polymer Battery - 3.7v 500mAh
Bike Gloves
Also check out these options for charging the LiPo battery.
Before Starting
If you are new to the Circuit Playground, you may want to first read these overview guides.
This project will use the Arduino IDE. Make sure you have added the board support for the Circuit Playground as well as installed the Circuit Playground library. MUST DO BOTH. This is covered in the guides linked above.
Bike Hand Signals
When riding a bicycle various hand signals are used to communicate your intentions to others sharing the road with you. This can be other bike riders, but also, and more importantly, to cars and trucks.
There are all kinds of bicycle hand signals, and they may vary from location to location. For a good overview, read the discussion on this web page:
For this project, we will focus on only two hand signals - the ones used to indicate turning direction. The ones we will use are shown below.
Bike Glove Assembly
Let's start by actually making the bike glove. This way you can upload programs to it as you work through the rest of the guide.
Use some double sided tape to attach the battery to the back of the Circuit Playground.
Attach the battery to the back of the Circuit Playground as shown.
Now get some needle and thread ready for sewing the Circuit Playground to the glove.
Sew the thread through the pad holes. Make several loops and then tie it off in a knot.
Two locations should be enough. I used the SCL #3 and #12 pad holes.
Done!
If you want, you can continue to wear the glove as you work through the guide. Just jack in to upload the sketches. You'll look totally cyberpunk!
Hand Position and Accelerometer
We will use the accelerometer to determine the hand position. For a good overview of the basics of how an accelerometer works, check out the How Tall Is It? guide. You can also read some technical details in the Lesson #0 Guide.
With the Circuit Playground sewn on the bike glove as in the previous section, the three main axis line up as shown in the image below.
Let's start by looking at the accelerometer output in the various hand positions. You can use the simple sketch below which will send the three accelerometer values to the serial port.
#include <Adafruit_CircuitPlayground.h>
float X, Y, Z;
void setup() {
Serial.begin(9600);
CircuitPlayground.begin();
}
void loop() {
X = CircuitPlayground.motionX();
Y = CircuitPlayground.motionY();
Z = CircuitPlayground.motionZ();
Serial.print(X);
Serial.print(",");
Serial.print(Y);
Serial.print(",");
Serial.println(Z);
delay(100);
}
With this sketch loaded and running on the Circuit Playground, open the Serial Plotter:
Tools -> Serial Plotter
You should see three lines being drawn, one for each axis of the accelerometer. Now move the glove into the three main positions:
Note how in each position there is one reading that stands out. For the hand down position it is the Z axis as reported by motionZ() . For the right turn position it is the X axis as reported by motionX() . For the left turn position it is the Y axis as reported by motionY() . So we can see a strong correlation between the hand positions of interest and the main axis of the accelerometer as:
So by simply checking the values of the various accelerometer readings, we can determine hand position. Let's see how next.
Hand Position Detection
The basic idea for detecting hand position is to check if the accelerometer values of each of the three axis exceed a preset level. This level is called a threshold. We will use three separate threshold values for the three separate axis values. This idea is shown in the image below.
Note that for the left turn, the value is negative.
Here is a program to demonstrates this. The threshold checks are done using if statements. Note that the if statements for the left turn/right turn checks are nested within the if statement for the hand down check. This is because the only time it makes sense to check for left/right is if the hand is up. We don't want the turn signal lights to go off while the hand is down on the handle bars.
///////////////////////////////////////////////////////////////////////////////
// Circuit Playground Bike Glove - Hand Position Detection
//
// Author: Carter Nelson
// MIT License (https://opensource.org/licenses/MIT)
#include <Adafruit_CircuitPlayground.h>
#define THRESHOLD_UP 5 // threshold for hand up test
#define THRESHOLD_RIGHT 5 // threshold for right turn
#define THRESHOLD_LEFT -5 // threshold for left turn
///////////////////////////////////////////////////////////////////////////////
void setup() {
Serial.begin(9600);
CircuitPlayground.begin();
}
///////////////////////////////////////////////////////////////////////////////
void loop() {
// check for hand up or down
if (CircuitPlayground.motionZ() > THRESHOLD_UP) {
Serial.println("HAND DOWN");
} else {
// check for right turn
if (CircuitPlayground.motionX() > THRESHOLD_RIGHT) {
Serial.println("RIGHT TURN");
// check for left turn
} else if (CircuitPlayground.motionY() < THRESHOLD_LEFT) {
Serial.println("LEFT TURN");
}
}
delay(500);
}
With this sketch loaded and running on the Circuit Playground, open up the Serial Monitor.
Tools -> Serial Monitor
You should see the current hand position printed out twice a second.
Try moving to the various hand positions and see how they are printed out as shown below.
Pretty simple, but it works.
Turn Signal Animations
OK, we got hand position detection working. However, car drivers aren't going to have the Serial Monitor running on their dashboards. So we should do something other than serial output. How about the NeoPixels?
We can replace the Serial.println() commands with code that will activate the NeoPixels. Even better, since this code will be in the main loop() function, it will be called over and over again. That way we can create some simple animations and let the main loop() function drive them.
Right Turn Animation
When the glove is in the 'right turn' orientation, the NeoPixels are arranged as shown in the image below.
What would be neat is if we could make an arrow pointing to the right. Something like this:
It won't be a perfect arrow, but what about using NeoPixels 2, 5, 6, 7, 8, and 9? Here's the code to test this out.
///////////////////////////////////////////////////////////////////////////////
// Circuit Playground Bike Glove - Right Turn Animation
//
// Author: Carter Nelson
// MIT License (https://opensource.org/licenses/MIT)
#include <Adafruit_CircuitPlayground.h>
#define BRIGHTNESS 255
#define RIGHT_COLOR 0xFFFFFF
#define ANIM_DELAY 200
///////////////////////////////////////////////////////////////////////////////
void rightTurnAnimation() {
// just to be sure, turn off all NeoPixels
CircuitPlayground.clearPixels();
// turn on NeoPixels to make an arrow shape
CircuitPlayground.setPixelColor(2, RIGHT_COLOR);
CircuitPlayground.setPixelColor(5, RIGHT_COLOR);
CircuitPlayground.setPixelColor(6, RIGHT_COLOR);
CircuitPlayground.setPixelColor(7, RIGHT_COLOR);
CircuitPlayground.setPixelColor(8, RIGHT_COLOR);
CircuitPlayground.setPixelColor(9, RIGHT_COLOR);
// wait a little bit
delay(ANIM_DELAY);
// turn them all off
CircuitPlayground.clearPixels();
// wait again
delay(ANIM_DELAY);
}
///////////////////////////////////////////////////////////////////////////////
void setup() {
CircuitPlayground.begin(BRIGHTNESS);
}
///////////////////////////////////////////////////////////////////////////////
void loop() {
rightTurnAnimation();
}
The functions rightTurnAnimation() does one 'frame' of the animation. Then, it is called over and over again by being placed in the loop() function.
Does this look like an arrow to you? Maybe. Kind of? Well, for now we'll just go ahead and use this as our right turn animation.
Left Turn Animation
When the glove is in the 'left turn' orientation, the NeoPixels are arranged as shown in the image below.
This is rotated from the right turn orientation, so the NeoPixels are arranged differently. In this arrangement, trying to make a left arrow is a bit of an issue.
Hmmmm. There are only a couple of the NeoPixels that seem to form an arrow. Maybe it would be enough to just use 8, 9, 0, and 1. But let's try something different for the left turn animation. We can make a neat chaser effect and light up the NeoPixels one at a time, moving from right to left. So first 5 & 4, then 6 & 3, then 7 & 2, then 8 & 1, and finally 9 & 0. Something like this:
Here's the code to test this out.
///////////////////////////////////////////////////////////////////////////////
// Circuit Playground Bike Glove - Left Turn Animation
//
// Author: Carter Nelson
// MIT License (https://opensource.org/licenses/MIT)
#include <Adafruit_CircuitPlayground.h>
#define BRIGHTNESS 255
#define LEFT_COLOR 0xFFFFFF
#define ANIM_DELAY 200
///////////////////////////////////////////////////////////////////////////////
void leftTurnAnimation() {
// just to be sure, turn off all NeoPixels
CircuitPlayground.clearPixels();
// Turn on 5 & 4
CircuitPlayground.setPixelColor(5, LEFT_COLOR);
CircuitPlayground.setPixelColor(4, LEFT_COLOR);
delay(ANIM_DELAY);
CircuitPlayground.clearPixels();
// Turn on 6 & 3
CircuitPlayground.setPixelColor(6, LEFT_COLOR);
CircuitPlayground.setPixelColor(3, LEFT_COLOR);
delay(ANIM_DELAY);
CircuitPlayground.clearPixels();
// Turn on 7 & 2
CircuitPlayground.setPixelColor(7, LEFT_COLOR);
CircuitPlayground.setPixelColor(2, LEFT_COLOR);
delay(ANIM_DELAY);
CircuitPlayground.clearPixels();
// Turn on 8 & 1
CircuitPlayground.setPixelColor(8, LEFT_COLOR);
CircuitPlayground.setPixelColor(1, LEFT_COLOR);
delay(ANIM_DELAY);
CircuitPlayground.clearPixels();
// Turn on 9 & 0
CircuitPlayground.setPixelColor(9, LEFT_COLOR);
CircuitPlayground.setPixelColor(0, LEFT_COLOR);
delay(ANIM_DELAY);
CircuitPlayground.clearPixels();
}
///////////////////////////////////////////////////////////////////////////////
void setup() {
CircuitPlayground.begin(BRIGHTNESS);
}
///////////////////////////////////////////////////////////////////////////////
void loop() {
leftTurnAnimation();
}
Just like before, the leftTurnAnimation() function does one pass through the animation. Then it is called over and over by the main loop() .
This looks pretty cool, so let's use it for our left turns.
Bike Glove Software
Now let's bring it all together into our final code. We just add our animation functions to the Hand Position Detection code and then replace the Serial.println() statements with calls to our left/right turn animations.
And here it is:
///////////////////////////////////////////////////////////////////////////////
// Circuit Playground Bike Glove - With "On/Off"
//
// Author: Carter Nelson
// MIT License (https://opensource.org/licenses/MIT)
#include <Adafruit_CircuitPlayground.h>
#define THRESHOLD_UP 5 // threshold for hand up test
#define THRESHOLD_RIGHT 5 // threshold for right turn
#define THRESHOLD_LEFT -5 // threshold for left turn
#define BRIGHTNESS 255
#define LEFT_COLOR 0xFFFFFF
#define RIGHT_COLOR 0xFFFFFF
#define ANIM_DELAY 200
///////////////////////////////////////////////////////////////////////////////
void leftTurnAnimation() {
// just to be sure, turn off all NeoPixels
CircuitPlayground.clearPixels();
// Turn on 5 & 4
CircuitPlayground.setPixelColor(5, LEFT_COLOR);
CircuitPlayground.setPixelColor(4, LEFT_COLOR);
delay(ANIM_DELAY);
CircuitPlayground.clearPixels();
// Turn on 6 & 3
CircuitPlayground.setPixelColor(6, LEFT_COLOR);
CircuitPlayground.setPixelColor(3, LEFT_COLOR);
delay(ANIM_DELAY);
CircuitPlayground.clearPixels();
// Turn on 7 & 2
CircuitPlayground.setPixelColor(7, LEFT_COLOR);
CircuitPlayground.setPixelColor(2, LEFT_COLOR);
delay(ANIM_DELAY);
CircuitPlayground.clearPixels();
// Turn on 8 & 1
CircuitPlayground.setPixelColor(8, LEFT_COLOR);
CircuitPlayground.setPixelColor(1, LEFT_COLOR);
delay(ANIM_DELAY);
CircuitPlayground.clearPixels();
// Turn on 9 & 0
CircuitPlayground.setPixelColor(9, LEFT_COLOR);
CircuitPlayground.setPixelColor(0, LEFT_COLOR);
delay(ANIM_DELAY);
CircuitPlayground.clearPixels();
}
///////////////////////////////////////////////////////////////////////////////
void rightTurnAnimation() {
// just to be sure, turn off all NeoPixels
CircuitPlayground.clearPixels();
// turn on NeoPixels to make an arrow shape
CircuitPlayground.setPixelColor(2, RIGHT_COLOR);
CircuitPlayground.setPixelColor(5, RIGHT_COLOR);
CircuitPlayground.setPixelColor(6, RIGHT_COLOR);
CircuitPlayground.setPixelColor(7, RIGHT_COLOR);
CircuitPlayground.setPixelColor(8, RIGHT_COLOR);
CircuitPlayground.setPixelColor(9, RIGHT_COLOR);
// wait a little bit
delay(ANIM_DELAY);
// turn them all off
CircuitPlayground.clearPixels();
// wait again
delay(ANIM_DELAY);
}
///////////////////////////////////////////////////////////////////////////////
void setup() {
CircuitPlayground.begin(BRIGHTNESS);
}
///////////////////////////////////////////////////////////////////////////////
void loop() {
// check slide switch position
if (CircuitPlayground.slideSwitch()) {
// check for hand up or down
if (CircuitPlayground.motionZ() > THRESHOLD_UP) {
// do nothing
} else {
// check for right turn
if (CircuitPlayground.motionX() > THRESHOLD_RIGHT) {
rightTurnAnimation();
// check for left turn
} else if (CircuitPlayground.motionY() < THRESHOLD_LEFT) {
leftTurnAnimation();
}
}
}
}
"ON/OFF" Switch
You may have noticed one extra feature added to this final code. Within the loop() function, everything is wrapped in an if statement that checks the position of the slide switch using CircuitPlayground.slideSwitch() . Like this:
void loop() {
// check slide switch position
if (CircuitPlayground.slideSwitch()) {
// MAIN CODE HERE
}
}
This was done to provide a simple on/off capability. If the Circuit Playground had an on/off switch for power, then we could just use that and turn it off for real. But since it doesn't we can use the slide switch. The Circuit Playground is still powered, but the code that makes the bike glove work is only run if the slide switch is in the + position.
Therefore:
Maybe you want to stop and pet a cute kitty you see, but don't want to freak it out with flashing lights. So you can just disable the lights real quick by sliding the switch to - position. Slide bike to + position when you're ready to go.
Happy riding!
Questions and Code Challenges
The following are some questions related to this project along with some suggested code challenges. The idea is to provoke thought, test your understanding, and get you coding!
While the sketches provided in this guide work, there is room for improvement and additional features. Have fun playing with the provided code to see what you can do with it. Or do something new and exciting!
Questions
Code Challenges