Maker.io main logo

Bluetooth based PIR motion detecting application using STM32 board

57

2022-08-23 | By Sheikh Shuhad

License: General Public License

1. Introduction

In this project we will use a PIR sensor to detect motion. Once motion is detected, it will trigger an interrupt and the BleuIO dongle connected to the board will advertise for 25 seconds. You can expand the project based on your needs further.

A PIR (passive infrared) Sensor is an electronic device that detects heats from human or animal body, giving a detection signal when movement happens in a given area or range of the sensor.

For this project, we will need one dongle and a PIR sensor (for example: https://www.digikey.com/short/4v12z2nw). When the BleuIO Dongle is connected to the Nucleo boards USB port the STM32 will recognize it and set up a new device name for the dongle: BleuIO PIR Detected. This will show up when the dongle is advertising.

2. Using the example project2.1 What we will need

2. How to setup project 2.1 Downloading the project from GitHub

Get project HERE https://github.com/smart-sensor-devices-ab/stm32_bleuio_pir_example Either clone the project, or download it as a zip file and unzip it, into your STM32CubeIDE workspace.

2.2 Importing as an Existing Project

  • From STM32CubeIDE choose File>Import…

Bluetooth based PIR application using STM32 board

  • Then choose General>Existing Projects into Workspace then click ‘Next >’

Bluetooth based PIR application using STM32 board

  • Make sure you’ve chosen your workspace in ‘Select root directory:’
  • You should see the project “stm32_bleuio_pir_example”, check it and click ‘Finish’.

Bluetooth based PIR application using STM32 board

 if you download the project as a zip file you will need to rename the project folder from ‘stm32_bleuio_pir_example-master’ to ‘stm32_bleuio_pir_example’

5. Connecting the sensor

Bluetooth based PIR application using STM32 board

Connect the PIR Sensor Gnd to ground and Vdd to power and Output to a pin of your choice on the Nucleo board (In the example we use PA0)

If you want a different PIN you will need to go into the STM32Cube ioc file and make some edits:

  • Click on PA0 and select Reset_State in the STM32Cube ioc file.
  • Click on your desired Pin and select EXTIO

Bluetooth based PIR application using STM32 board

Bluetooth based PIR application using STM32 board

  • Then go to GPIO under System Core and make sure you setup the pin as follows:GPIO mode: External Interrupt Mode with Rising edge trigger detectionGPIO Pull-up/Pull-down: Pull-down

Bluetooth based PIR application using STM32 board

  • Then go to NVIC under System Core and make sure EXTI line0 interrupt is enabled

Bluetooth based PIR application using STM32 board

 

6. Running the example

  • In STMCubeIDE click the hammer icon to build the project.
  • Open up the ‘STMicroelectronics STLink Viritual COM Port’ with a serial terminal emulation program like TeraTerm, Putty or CoolTerm.

Baudrate: 115200

Data Bits: 8

Parity: None

Stop Bits: 1

Flow Control: None

  • In STMCubeIDE click the green play button to flash and run it on your board. The first time you click it the ‘Run Configuration’ window will appear. You can just leave it as is and click run.
  • Connect the BleuIO Dongle.

7. Output

When the PIR sensor detects movement it will trigger an interrupt that in turn will tell the BleuIO Dongle to advertise for 25 seconds. Just so the PIR Sensor will not trigger constantly we have put a 20 second timeout before it will trigger again. If no new interrupts have been detected after the 25 second advertising timer has run out the BleuIO Dongle will stop advertising and wait for a new interrupt to happen.

Bluetooth based PIR application using STM32 board

Bluetooth based PIR application using STM32 board

The yellow LED on the STM32 board also toggles if there is a movement.

Hope you found this article informative.

制造商零件编号 SSD005/4-V2B
BLUETOOTH 5 LOW ENERGY USB DONGL
Smart Sensor Devices
制造商零件编号 SSD005/4-V2W
BLUETOOTH 5 LOW ENERGY USB DONGL
Smart Sensor Devices
制造商零件编号 EKMB1301111K
SENSOR PIR
Panasonic Electric Works
制造商零件编号 NUCLEO-H743ZI2
NUCLEO-144 STM32H743ZI EVAL BRD
STMicroelectronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.