Maker.io main logo

Li-Fi data transfer experiment - transferring data using a Led and Solar

2023-08-28 | By Mirko Pavleski

License: GNU Lesser General Public License Arduino

 

In this experiment I will describe you a way where the light from 10W Power LED diode is used for transferring Audio signal wirelessly.

1

LED bulbs are semiconductor devices, which means the current, and therefore the illumination can be modulated at extremely high speeds which can be detected by the photodetector.

 

Using this technique allows for high-speed information can be transmitted from an LED light bulb. So, the same light energy used for illumination may also be used for communication.

2

In this experiment I will describe you a way where the light from 10W Power LED diode is used for this purpose as a medium of transmission. To reduce the losses at the lowest level, we direct light from the source through a plane convex lens, so if the light source is positioned exactly at the focal point, the light rays on the exit will extend almost parallel and directly hit the receiver (solar cell) with the least loss.

44

In this way, the distance at which transmission can be carried out is drastically increased, and at the same time, due to the strong intensity of light that reaches the receiver, the influence of the ambient light has an insignificant effect. As I mentioned earlier, the experiment is very simple to replicate and consists of several parts:

5

- The transmitter, which consists of an LED that is mounted on a suitable heatsink and can be moved in this channel to position it exactly on the focal point.

6

- This small electronic board is a modulator, whose task is to incorporate the audio signal into the light source. It consists of only one mosfet and a few passive elements, and the schematic is given below.

7

- And a DC voltage source that powers the transmitter.

8

- The receiver is actually a solar cell, in my case two elements that generate 5 volts each connected in series, but this is not critical and any panel we have at hand can be used. The signal from the solar panel is fed to the Aux input of this small radio receiver through a 10-microfarad capacitor, whose function is to not pass the DC component of the signal. Otherwise, this radio in this case has the function of an audio amplifier. Now let's see how the device works in reality: First we turn on the transmitter and focus the output beam. An audio signal is brought to the input of the modulator, in my case from the sound card of the personal computer. On the side of the receiver, we turn on the radio, then we select the Aux input. The signal from the transmitter is emitted on the receiver. If we block the light beam, the transfer is interrupted.

9

The distance between the transmitter and the receiver can be increased up to a certain limit that depends on several parameters. In our case it is a maximum of 5 to 6 meters with acceptable signal attenuation. Next, I will present you a practical example of transmitting an audio signal through a room lighting source. We connect the lighting through a modulator, and a small solar panel is connected to the receiver.

10

Now if I feed a music signal to the input of the modulator, that same signal will be output to the radio. Many different signals can be transmitted in the same way, such as the Internet, which is the most used service today. And finally, a short conclusion: First the positive aspects - As we could see and hear, the transfer is done without any distortions and degradation of the original signal. - Since homes and offices already have LED bulbs for lighting purposes, the same source of light can be used to transmit data. - Quicker Data Transmission than Wi-Fi - One main advantage of Li-Fi is security. Since light cannot pass through opaque structures, Li-Fi Internet for example is available only to the users within a room and cannot be breached by users in other rooms or buildings. On the other hand, the biggest disadvantages are: - Because it uses visible light, and light cannot penetrate walls, the signal's range is limited by physical barriers - Other sources like sunlight may interfere with the signal. - A whole new infrastructure for Li-Fi would need to be constructed. Otherwise, initially my idea for this experiment was to achieve wireless power transfer, i.e. wireless transmission of electricity using light rays but unfortunately, the utilization rate is extremely low, and practically of this method is unusable. As we can see from this example, the utilization of a distance of 50cm is less than one percent.

12

Currently, in Norway, work is being done on the development of a photovoltaic panel (receiver) for laser homogeneous light that has a useful coefficient greater than 80 percent (in today's solar cells it is at most 20 percent), whereby energy transfer over long distances will be practically applicable. In one of the following videos, I will present data transmission via Li-Fi using an Arduino microcontroller.

13

TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum