制造商零件编号 3333
CIRCUIT PLAYGROUND EXPRESS
Adafruit Industries LLC
License: See Original Project Circuit Playground
Courtesy of Adafruit
Guide by John Park
Overview
You can use your Circuit Playground Express (CPX) to build a fun, interactive, and beautiful holiday snow globe! Using CircuitPython, you can code the CPX to read its built-in accelerometer and detect when the snow globe is being shaken, and then play back a melody and festive light show!!
Materials and Parts
Besides the electronics listed below, you'll also need:
Code with CircuitPython
You'll code your snow globe using CircuitPython. You'll be able to use the built-in accelerometer to detect when the snow globe is shaken, and then play a light show on the NeoPixels and play simple songs with the built-in speaker.
Get Ready!
Download the Snow Globe Python Code
Copy the code below, and paste it into a new text document in your text editor, or in the Mu code editor for CircuitPython.
# Snow Globe
# for Adafruit Circuit Playground express
# with CircuitPython
from adafruit_circuitplayground.express import cpx
import math
import time
ROLL_THRESHOLD = 30 # Total acceleration
cpx.pixels.brightness = 0.1 # set brightness value
WHITE = (65, 65, 65)
RED = (220, 0, 0)
GREEN = (0, 220, 0)
BLUE = (0, 0, 220)
SKYBLUE = (0, 20, 200)
BLACK = (0, 0, 0)
# Initialize the global states
new_roll = False
rolling = False
def fade_pixels(fade_color): # pick from colors defined above, e.g., RED, GREEN, BLUE, WHITE, etc.
# fade up
for j in range(25):
pixel_brightness = (j * 0.01)
cpx.pixels.brightness = pixel_brightness
for i in range(10):
cpx.pixels[i] = fade_color
# fade down
for k in range(25):
pixel_brightness = (0.25 - (k * 0.01))
cpx.pixels.brightness = pixel_brightness
for i in range(10):
cpx.pixels[i] = fade_color
# fade in the pixels
fade_pixels(GREEN)
def play_song(song_number):
# 1: Jingle bells
# 2: Let It Snow
# set up time signature
whole_note = 1.5 # adjust this to change tempo of everything
# these notes are fractions of the whole note
half_note = whole_note / 2
quarter_note = whole_note / 4
dotted_quarter_note = quarter_note * 1.5
eighth_note = whole_note / 8
# set up note values
A3 = 220
Bb3 = 233
B3 = 247
C4 = 262
Db4 = 277
D4 = 294
Eb4 = 311
E4 = 330
F4 = 349
Gb4 = 370
G4 = 392
Ab4 = 415
A4 = 440
Bb4 = 466
B4 = 494
if song_number == 1:
# jingle bells
jingle_bells_song = [[E4, quarter_note], [E4, quarter_note],
[E4, half_note], [E4, quarter_note], [E4, quarter_note],
[E4, half_note], [E4, quarter_note], [G4, quarter_note],
[C4, dotted_quarter_note], [D4, eighth_note], [E4, whole_note]]
for n in range(len(jingle_bells_song)):
cpx.start_tone(jingle_bells_song[n][0])
time.sleep(jingle_bells_song[n][1])
cpx.stop_tone()
if song_number == 2:
# Let It Snow
let_it_snow_song = [[B4, dotted_quarter_note], [A4, eighth_note],
[G4, quarter_note], [G4, dotted_quarter_note], [F4, eighth_note],
[E4, quarter_note], [E4, dotted_quarter_note], [D4, eighth_note],
[C4, whole_note]]
for n in range(len(let_it_snow_song)):
cpx.start_tone(let_it_snow_song[n][0])
time.sleep(let_it_snow_song[n][1])
cpx.stop_tone()
play_song(1) # play music on start
# Loop forever
while True:
# check for shaking
# Compute total acceleration
x_total = 0
y_total = 0
z_total = 0
for count in range(10):
x, y, z = cpx.acceleration
x_total = x_total + x
y_total = y_total + y
z_total = z_total + z
time.sleep(0.001)
x_total = x_total / 10
y_total = y_total / 10
z_total = z_total / 10
total_accel = math.sqrt(x_total*x_total + y_total*y_total + z_total*z_total)
# Check for rolling
if total_accel > ROLL_THRESHOLD:
roll_start_time = time.monotonic()
new_roll = True
rolling = True
print('shaken')
# Rolling momentum
# Keep rolling for a period of time even after shaking stops
if new_roll:
if time.monotonic() - roll_start_time > 2: # seconds to run
rolling = False
# Light show
if rolling:
fade_pixels(SKYBLUE)
fade_pixels(WHITE)
cpx.pixels.brightness = 0.8
cpx.pixels.fill(WHITE)
elif new_roll:
new_roll = False
# play a song!
play_song(2)
#return to resting color
fade_pixels(GREEN)
cpx.pixels.brightness = 0.05
cpx.pixels.fill(GREEN)
Now, save the code onto your Circuit Playground Express as main.py
The board will restart once the code has been saved. You'll see the pixels fade up green, and then a song plays.
Now, you can shake the board to start the snowfall light sequence, followed by a second song. Finally, it will fade back to green, awaiting the next time it is shaken.
Here's how the code works!
Snowy Code!
There are three basic things we need for our code to do:
Using the Circuit Playground Express library
In CircuitPython on the Circuit Playground Express, we can do most of these things with high-level commands, such as:
cpx.pixels.fill(255, 0, 0)
to make all of the NeoPixels turn red, or:
cpx.start_tone(440)
to play an A4 music note.
(These commands are made possible by the use of the Circuit Playground Express library which is part of the library bundle you installed.)
With the library available on the board, you can then import it into your code with this line:
from adafruit_circuitplayground.express import cpx
Now, you can use a number of commands that simplify and make consistent the ways you work with the board. Most functions, such as reading the buttons and sensors, to lighting NeoPixels, and playing tones and .wav files have a cpx command available.
A Tour of the Code
Let's have a look at the code in small chunks before we save the entire program to the board.
First, we'll import the libraries to give us access to simpler, higher level commands that we'll need.
# Snow Globe
# Circuit Playground Express
from adafruit_circuitplayground.express import cpx
import math
import time
Next, we'll set up a variable called ROLL_THRESHOLD that determines how hard we'll need to shake the snow globe to activate it.
We'll also set the total brightness of the NeoPixels, and create color names to control the red, green, and blue values of the LEDs without needing to write in the numerical values each time.
ROLL_THRESHOLD = 30 # Total acceleration
cpx.pixels.brightness = 0.1 # set brightness value
WHITE = (65, 65, 65)
RED = (220, 0, 0)
GREEN = (0, 220, 0)
BLUE = (0, 0, 220)
SKYBLUE = (0, 20, 200)
BLACK = (0, 0, 0)
Fading Pixels
In order to make our code efficient, we'll create a function named fade_pixels that controls the fade up and fade down of NeoPixels. We can call this function, along with one of our pre-defined color names, any time we need to animate the lights later on.
The contents of this function are two loops, one for fade up and a second for fade down. Let's look at the fade up loop (they both work essentially the same way).
The line for j in range(25): is a loop that iterates the code below it that is indented in a level 25 times. Each time, it increments the value of j by one, so j starts at 0 and ends at 24.
The code that is iterated is an increase of the pixel_brightness variable:
pixel_brightness = (j * 0.01)
So, this starts out as 0 and steps through to a value of 0.24
This number is then applied to the NeoPixels overall in the next line:
cpx.pixels.brightness = pixel_brightness
Then, each of the ten NeoPixel is set to the specified fade_color with the next loop for i in range(10): which iterates over the line cpx.pixels[i] = fade_color
def fade_pixels(fade_color): # pick from colors defined above, e.g., RED, GREEN, BLUE, WHITE, etc.
# fade up
for j in range(25):
pixel_brightness = (j * 0.01)
cpx.pixels.brightness = pixel_brightness
for i in range(10):
cpx.pixels[i] = fade_color
# fade down
for k in range(25):
pixel_brightness = (0.25 - (k * 0.01))
cpx.pixels.brightness = pixel_brightness
for i in range(10):
cpx.pixels[i] = fade_color
Playing a Song
The next function definition is play_song() which is used to play one of two songs coded within, Jingle Bells or Let It Snow. You could write other songs and add them!
First, we create a variable called whole_note to define the length of a whole note, in this case, 1.5 seconds. You can adjust that to increase or decrease the tempo. All other note lengths are derived from this one variable, e.g. half_note is a whole_note * 0.5
Similarly, we create a series of variables to define the pitches different notes, starting from A3 up to B4. This way, we can call the command cpx.start_tone() with a note name instead of a frequency value. This makes it much easier to transcribe from standard music notation!
def play_song(song_number):
# 1: Jingle bells
# 2: Let It Snow
# set up time signature
whole_note = 1.5 # adjust this to change tempo of everything
# these notes are fractions of the whole note
half_note = whole_note / 2
quarter_note = whole_note / 4
dotted_quarter_note = quarter_note * 1.5
eighth_note = whole_note / 8
# set up note values
A3 = 220
Bb3 = 233
B3 = 247
C4 = 262
Db4 = 277
D4 = 294
Eb4 = 311
E4 = 330
F4 = 349
Gb4 = 370
G4 = 392
Ab4 = 415
A4 = 440
Bb4 = 466
B4 = 494
Playing one note
To play one note, say a C, for a quarter note duration, we'll start the tone, sleep for a quarter note, and stop the tone. It will look like this:
cpx.start_tone(C4)
time.sleep(qN)
cpx.stop_tone()
Playing many notes
There are a couple of ways to transcribe a song using this method. The first way is very clear, but uses many lines of code:
if song_number == 1:
# jingle bells
for i in range(2): # repeat twice
# jingle bells...
cpx.stop_tone()
cpx.start_tone(E4)
time.sleep(qN)
cpx.stop_tone()
cpx.start_tone(E4)
time.sleep(qN)
cpx.stop_tone()
cpx.start_tone(E4)
time.sleep(hN)
cpx.stop_tone()
# jingle all the way
cpx.start_tone(E4)
time.sleep(qN)
cpx.stop_tone()
cpx.start_tone(G4)
time.sleep(qN)
cpx.stop_tone()
cpx.start_tone(C4)
time.sleep(dqN)
cpx.stop_tone()
cpx.start_tone(D4)
time.sleep(eN)
cpx.stop_tone()
cpx.start_tone(E4)
time.sleep(wN)
cpx.stop_tone()
That's very straightforward -- other than looping the initial phrase twice, it repeats three commands over and over again for every note of the song. You can imagine that this would get really long, quickly!
The second method involves packing the entire set of notes and durations into a two-dimensional array, like this:
# jingle bells
jingle_bells_song = [[E4, quarter_note], [E4, quarter_note],
[E4, half_note], [E4, quarter_note], [E4, quarter_note],
[E4, half_note], [E4, quarter_note], [G4, quarter_note],
[C4, dotted_quarter_note], [D4, eighth_note], [E4, whole_note]]
You can see how each pair in the list is a note pitch, followed by its play duration.
We can then play that song with a few lines of code that iterate through the array, playing and pausing for the values one pair at a time:
for n in range(len(jingle_bells_song)):
cpx.start_tone(jingle_bells_song[n][0])
time.sleep(jingle_bells_song[n][1])
cpx.stop_tone()
Also, note how the number of times needed to iterate through the loop is derived from querying the length of the jingle_bells_song array with the len() command. This way the number of iterations will always match the number of notes we add to or subtract from the song. If we were to instead hard code it with the number of notes like this: for n in range(11) we would need to constantly update that value while working on the song. No fun!
Then, we'll define a second song, Let It Snow:
if song_number == 2:
# Let It Snow
let_it_snow_song = [[B4, dotted_quarter_note], [A4, eighth_note],
[G4, quarter_note], [G4, dotted_quarter_note], [F4, eighth_note],
[E4, quarter_note], [E4, dotted_quarter_note], [D4, eighth_note],
[C4, whole_note]]
Once all of that has been defined, we'll play through Jingle Bells once:
play_song(1) # play music on start
Main Loop!
Now, we get to the main loop, this is what will repeat over and over again.
The first thing to do is set up some variables and math to compute total acceleration from movement on all three axes of the accelerometer.
while True:
# check for shaking
# Compute total acceleration
x_total = 0
y_total = 0
z_total = 0
for count in range(10):
x, y, z = cpx.acceleration
x_total = x_total + x
y_total = y_total + y
z_total = z_total + z
time.sleep(0.001)
x_total = x_total / 10
y_total = y_total / 10
z_total = z_total / 10
total_accel = math.sqrt(x_total*x_total + y_total*y_total + z_total*z_total)
Now, we'll have the total_accel value to compare to a threshold of 30 that we set at the top of the program called ROLL_THRESHOLD.
# Check for rolling
if total_accel > ROLL_THRESHOLD:
roll_start_time = time.monotonic()
new_roll = True
rolling = True
print('shaken')
# Rolling momentum
# Keep rolling for a period of time even after shaking stops
if new_roll:
if time.monotonic() - roll_start_time > 2: # seconds to run
rolling = False
When shaking is detected, we will run the fade_pixels function twice, first with sky blue, and then with white. We'll then fill all pixels with a bright white!
# Light show
if rolling:
fade_pixels(SKYBLUE)
fade_pixels(WHITE)
cpx.pixels.brightness = 0.8
cpx.pixels.fill(WHITE)
Lastly, when the shaking has stopped, we'll play the second song and then fade_pixels to green.
elif new_roll:
new_roll = False
# play a song!
play_song(2)
#return to resting color
fade_pixels(GREEN)
cpx.pixels.brightness = 0.05
cpx.pixels.fill(GREEN)
From this point, the snow globe will stay lit green, waiting to be shaken again!
Make the Snow Globe
Globe Preparation
Begin by preparing the snow globe. First, you'll fill it nearly to the top with distilled water.
Next, to make the water more viscous, and give the glitter snowflakes more hang time, add 2 tsp. of glycerin to the water and stir it up well to incorporate.
Now, it's glitter time! You can choose the color and amount to suit -- I used 1 tsp. of white and 1/2 tsp. of silver. Add it to the water and stir.
Pretty! Shiny!!
Electronics
Next, we'll add the electronics to the globe. The lid area is completely dry -- separated from the globe's water by the plug, which we'll add later, including an adhesive seal for safety.
Battery Power
Using a screwdriver, remove the belt clip from your AAA battery pack. We'll use the pack as a base, so we need it to be flat.
Insert the batteries into the pack and close the lid.
Connect the JST plug to the Circuit Playground Express and then affix the board to the inside of the lid with double stick foam tape.
The lid and Circuit Playground Express are now ready to be screwed into place later, once we've added our figurine to the snow globe.
Add the Figurine
You can choose anything water resistant you like to display within your snow globe! LEGO figures, tiny horses, a collection of cursed D20 dice, it's really up to you!
I decided to 3D print an AdaBot figurine. This one was created by the Ruiz Bros. for the Adafruit Chess Set. I modified the base slightly so that it would be a smaller diameter and allow more light in from the bottom, as that's where our NeoPixels are.
You can download the files here and print them if you like.
After printing, I painted Adabot's lightning bolt and eyes with some acrylic paint and a small brush, then sealed it with spray lacquer when it was dry.
I used a bit of CA glue to join the two halves.
Attach the Figure to the Plug
You can use E6000 (or Goop) adhesive to glue the base of your figure to the top of the snow globe's plug, then let it dry, up to 24 hours
Take the Plunge
When the figure's glue has dried, it's time to make it take the plunge!
First, make sure you do this over a sink or bowl! Push the figure and plug down slowly, displacing any water to get a nice, full globe. If there's too much air, add water.
The plug is held in place by the pressure of the lid, but it's best to seal it with some glue or caulking just to be sure there are no leaks. I used more E6000 here.
Screw on the Lid
Once the plug's glue has dried and you confirm that it's well sealed from any leaks, you can screw on the lid/Circuit Playground Express/battery pack.
Use the Snow Globe
Congratulations! You've built your CircuitPython Snow Globe, and now it's time to shake it up and enjoy!
Turn on the battery pack's switch. The lights will come up, and you'll be treated to a song.
Pick it up and give it a good shake!
Enjoy the lights and snowfall.
Finally, another song plays, and the lights return to the festive green!