Shake2Wake click
Shake2Wake click carries an ADXL362 ultralow power, 3-axis MEMS accelerometer from Analog Devices. The distinguishing feature of this IC is that it incorporates several activity detection modes. The interrupt pins from the chip are connected to an onboard ADP195 power switch IC that in turn controls an external device connected through a screw terminal. The detection threshold is configurable (both intensity and duration). The duration of inactivity that leads to switching off is also programmable. Shake2Wake click can also be used as a regular accelerometer, for continuous sensing, in which case it communicates with the target MCU through mikroBUS™ SPI interface. Uses 3.3V power supply only.