VideoLibrary
How to Select a Wireless Connectivity Solution – ATM | DigiKey
Wireless communication has advanced by leaps and bounds since the first devices shed their communication cables and wires. Now designers have many wireless communications options depending on their needs for range, low cost or security.
Video Player is loading.
Current Time 0:00
Duration 0:00
Loaded: 0%
Stream Type LIVE
Remaining Time 0:00
 
1x
  • Chapters
  • descriptions off, selected
  • subtitles off, selected

      How to Select a Wireless Connectivity Solution – ATM | DigiKey

      So, you want to go wireless and but you are not sure which technology to embrace. The key factors and limitations are demonstrated in this video to help in selecting which is right for your project. Factors such as cost, range, security and ease of implementation are covered to pare down the wide array of options. There was a time when remote control still involved a cable tether to pass signals from the user to a device such as a toy car, television or telephones which were bulky and usually attached to a wall or placed on a desk with long, unsightly cords to drag around. The latest technologies broadcast signals everywhere while targeting specific receivers that do not rely on line-of-sight methods.

      1/29/2024 4:19:55 PM