The International Standard IEC 60529 outlines an international classification system that describes the sealing characteristics of electrical equipment. The classification system defines the level of protection provided by enclosures to prevent the ingress of foreign objects and moisture into the electrical equipment. Under this classification, snap-action switches mainly come within the following categories: IP40 with insulated connections when no indication or IP65, IP66, IP67, IP69 sealed snap switches, as indicated.