制造商零件编号 2821
ESP8266 FEATHER HUZZAH LOOSE HDR
Adafruit Industries LLC
License: See Original Project Arduino Adafruit Feather
Courtesy of Adafruit
Guide by Todd Treece
Overview
This guide is part of a series of guides that cover the basics of using Adafruit IO. It will show you how to send analog values to Adafruit IO from a photocell.
If you haven't worked your way through the Adafruit IO feed and dashboard basics guides, you should do that before continuing with this guide so you have a basic understanding of Adafruit IO.
You should go through the setup guides associated with your selected set of hardware, and make sure you have internet connectivity with the device before continuing.
If you have went through all of the prerequisites for your selected hardware, you are now ready to move on to the Adafruit IO setup steps that are common between all of the hardware choices for this project. Let's get started!
Adafruit IO Setup
The first thing you will need to do is to login to Adafruit IO and visit the Settings page.
Click the VIEW AIO KEY button to retrieve your key.
A window will pop up with your Adafruit IO. Keep a copy of this in a safe place. We'll need it later.
Creating the Analog Feed
Next, you will need to create a feed called Analog. If you need help getting started with creating feeds on Adafruit IO, check out the Adafruit IO Feed Basics guide.
Adding the Gauge Block
Next, add a new Gauge block to a new or existing dashboard. Name the block whatever you would like, and give it a max value of 1024 and a min value of 0. Make sure you have selected the Analog feed as the data source for the gauge.
If you need help getting started with Dashboards on Adafruit IO, check out the Adafruit IO Dashboard Basics guide.
When you are finished editing the form, click Create Block to add the new block to the dashboard.
Next, we will look at wiring the circuit.
Wiring
You will need the following parts for this tutorial:
You will need to connect the following pins to the photocell and 10k resistor:
Note: Resistors and photocells are not polarized, so they can be connected to the circuit in either direction.
Next, let's look at the example sketch we will be using.
Arduino Setup
You should go through the setup guides associated with your selected set of hardware, and make sure you have internet connectivity with the device before continuing.
You will need to make sure you have at least version 2.3.0 of the Adafruit IO Arduino library installed before continuing.
For this example, you will need to open the adafruitio_08_analog_in example in the Adafruit IO Arduino library.
Next, we will look at the network configuration options in the sketch.
Network Config
To configure the network settings, click on the config.h tab in the sketch. You will need to set your Adafruit IO username in the IO_USERNAME define, and your Adafruit IO key in the IO_KEY define.
WiFi Config
WiFi is enabled by default in config.h so if you are using one of the supported WiFi boards, you will only need to modify the WIFI_SSID and WIFI_PASS options in the config.h tab.
FONA Config
If you wish to use the FONA 32u4 Feather to connect to Adafruit IO, you will need to first comment out the WiFi support in config.h
Next, remove the comments from both of the FONA config lines in the FONA section of config.h to enable FONA support.
Ethernet Config
If you wish to use the Ethernet Wing to connect to Adafruit IO, you will need to first comment out the WiFi support in config.h
Next, remove the comments from both of the Ethernet config lines in the Ethernet section of config.h to enable Ethernet Wing support.
Next, we will look at how the example sketch works.
Code
The adafruitio_08_analog_in example uses pin A0 by default on all boards, and that can be modified if needed by changing the PHOTOCELL_PIN define.
/************************ Example Starts Here *******************************/
// analog pin 0
#define PHOTOCELL_PIN A0
The next chunk of code sets up two integer variables to track the state of the photocell, and an Adafruit IO Feed instance for a feed called analog.
// photocell state
int current = 0;
int last = -1;
// set up the 'analog' feed
AdafruitIO_Feed *analog = io.feed("analog");
The setup function connects your feather to Adafruit IO. The code will wait until you have a valid connection to Adafruit IO before continuing with the sketch. If you have any issues connecting, check config.h for any typos in your username or key.
void setup() {
// start the serial connection
Serial.begin(115200);
// wait for serial monitor to open
while(! Serial);
// connect to io.adafruit.com
Serial.print("Connecting to Adafruit IO");
io.connect();
// wait for a connection
while(io.status() < AIO_CONNECTED) {
Serial.print(".");
delay(500);
}
// we are connected
Serial.println();
Serial.println(io.statusText());
}
Next, we have the main loop() function. The first line of the loop function calls io.run(); this line will need to be present at the top of your loop in every sketch. It helps keep your device connected to Adafruit IO, and processes any incoming data.
void loop() {
// io.run(); is required for all sketches.
// it should always be present at the top of your loop
// function. it keeps the client connected to
// io.adafruit.com, and processes any incoming data.
io.run();
The next chunk of code inside the loop() checks the current value of the photocell, and saves the value of the photocell in the current variable.
We then check if the current photocell value is equal to the last photocell value. If it is equal, we will return early and not continue with the rest of the loop.
// grab the current state of the photocell
current = analogRead(PHOTOCELL_PIN);
// return if the value hasn't changed
if(current == last)
return;
The final chunk of the loop() function prints the current value to the Arduino Serial Monitor, and sends the current value to the analog feed on Adafruit IO. We also set last = current; so we can tell if the value of the photocell has changed in the next run of the loop.
// save the current state to the analog feed
Serial.print("sending -> ");
Serial.println(current);
analog->save(current);
// store last photocell state
last = current;
// wait one second (1000 milliseconds == 1 second)
delay(1000);
}
Upload the sketch to your board, and open the Arduino Serial Monitor. Your board should now connect to Adafruit IO.
Connecting to Adafruit IO....
Adafruit IO connected.
You can now cover the photocell with your hand, and you should see the changing values being sent to Adafruit IO.
sending -> 1024
sending -> 953
sending -> 259
sending -> 476
sending -> 248
sending -> 173
sending -> 224
sending -> 291
sending -> 1024
Check your dashboard on Adafruit IO, and you should see the gauge respond to the changes in photocell values.