Maker.io main logo

The Bytesaber: A Sharpie Holder That Looks Like a Lightsaber Hilt

2023-06-23 | By Zach Hipps

License: See Original Project

089---The-Bytesaber

I have an impractical idea for a lightsaber hilt that can hold a Sharpie marker. My initial ‎concept involves attaching the Sharpie to the hilt using the small shoulder found just ‎above the marker's tip. To bring my vision to life, I started by 3D printing several ‎samples with different diameters. I needed to find the perfect size that would create a ‎good seal without drying out the pen. After a few tests, I discovered that a diameter of ‎either 5.60 or 5.65 millimeters would work best. Ultimately, I settled on 5.65 millimeters ‎as the ideal fit.‎

089 The Bytesaber 00 02 10 20

Now that the size issue is resolved, I can move on to designing the cylindrical hilt. My ‎plan is to create a standard hilt that is interchangeable, allowing for the customization ‎of different lightsaber styles. I intentionally left out the cool sci-fi-looking aesthetic ‎because that would be accomplished later on. To accommodate the Sharpie, I extruded ‎a hole into the top of the cylinder and added threads to allow for the attachment of ‎different tops. This design feature would enable the creation of unique lightsabers by ‎simply swapping out the top pieces.‎

089-The-Bytesaber 00_06_56_16

Originally, I had planned to manufacture the hilt using aluminum. However, the high cost quotes I received discouraged me from pursuing that option. Instead, I turned to ‎resin printing, which offered a more cost-effective alternative for this project. ‎Nevertheless, I still want to explore metal fabrication using a metal lathe in the future.‎

089-The-Bytesaber 00_07_20_20

089-The-Bytesaber 00_03_52_55

I want to incorporate LEDs into the Bytesaber, so I designed a circular PCB with a hole ‎in the middle, allowing the Sharpie to fit through while the lights would shine around it. ‎The PCB featured four LEDs and four resistors, evenly distributed in a radial pattern to ‎provide uniform lighting and was ordered through DigiKey’s DK Red PCB service. ‎Powering the LEDs required a sufficient forward voltage, which couldn't be supplied by ‎a standard AAA battery. I opted for a lithium-ion battery made from an 18650 cell which ‎is known for its energy density. The standardized hilt needs to include a compartment ‎to accommodate the battery and a cap to seal it. However, routing the negative wire ‎proved to be a challenge. To overcome this, I created a slot along the inner wall of the ‎battery compartment, allowing the wire to reach the negative terminal of the battery. ‎One crucial element I need to address is how to incorporate a switch to turn the lights ‎on and off without twisting the wires. I considered drilling a hole in the end cap, but it ‎dawned on me that it would cause twisting whenever the cap was screwed on or off. ‎This design flaw required further consideration and a creative solution.‎

089-The-Bytesaber 00_09_58_33

089-The-Bytesaber 00_07_57_23

In the meantime, I finished printing the interchangeable accessories to transform the ‎standard hilt into the Darth Vader lightsaber. It has a really cool top shroud with a ‎steep, cut-off angle and a very sinister grip with ribs running vertically. I spray painted ‎the standard hilt with a metallic silver color, and at this point, I’m ready to work on the ‎electronics. I applied solder paste to the custom PCBs I designed and placed the ‎resistors and LEDs by hand. My reflow station made quick work of melting the solder ‎paste and reflowing the components to the board. From there, I pulled some stranded ‎wire from the top of the hilt into the battery compartment. DigiKey stocks 18650 battery ‎cells with wires already soldered to the ends, but since I built my own battery packs ‎before, I had a bunch of materials left over and decided to build my own. I soldered ‎some wire to a small piece of nickel strip and used a spot welder to fasten the wire to ‎the positive battery terminal. I did the same for the negative terminal but included a ‎push button switch in line with the negative wire so that I can turn the LEDs on and off. ‎At this point, I came up with a solution to the twisting wires problem. I needed to design ‎an end cap with two lobes that mate with slots in the hilt. This way I can sort of use a ‎twist lock mechanism to secure the button to the bottom of the hilt. I completed ‎assembly by using hot glue to fasten the Darth Vader accessories to one standard hilt, ‎and Luke Skywalker accessories to the other standard hilt. The project wasn’t complete, ‎however. I didn’t want these awesome Bytesabers to just sit flat on my desk. They ‎warranted a bent sheet metal display stand to hold the Bytesabers at a near vertical ‎angle. And because there needs to be balance to the force, I included the Empire logo ‎on one display while the other display had the Rebel Alliance logo just for fun.‎

089-The-Bytesaber 00_12_05_08

‎Did I really need a nerdy way to hold my Sharpie collection on my desk? Of course not. ‎But as impractical as this project was, I can’t stop smiling every time I reach for a ‎Sharpie now.

089-The-Bytesaber 00_12_08_30

 

制造商零件编号 3175
HOOK-UP 22AWG STRAND - 10 X 25FT
Adafruit Industries LLC
制造商零件编号 RP8201B2M1CEBLKBLKNIL
SWITCH PUSH SPST 0.1A 24V
E-Switch
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.