NTU Fuzzy Circuits - LED Wallet/Purse
2024-07-18 | By Kitronik Maker
License: See Original Project LEDs / Discrete / Modules Wearables
Courtesy of Kitronik
Guide by Kitronik
A student studying Secondary Design and Technology Education at Nottingham Trent University designed a purse with built-in LED, fixing the age old issue of searching for bits of change in the dark.
In quoting Buechley, the student was ‘aiming to attract more women and girls’, and to ‘inspire and educate the next generation of scientists and engineers’. Aimed at Key Stage 3 pupils and therefore a simplified kit, the student aimed to find a way that students could use simple E-Textiles ideas in school, at a reasonable price.
Front of two LED wallet/purses
Using conductive thread, the student was able to make the purse with little traditional circuitry, keeping the cost and bulk of the purse/wallet down to a minimum. Conductive thread is a relatively new tool for making products, and for items such as this purse/wallet it is ideal for retaining a sense of style along with functionality, rather than trying to hide an electrical circuit and wires inside the lining and making the product too bulky.
Back of two LED wallet/purses
Parts required:
- 2 x A5 sheets of felt
- Small amount of conductive thread (for the battery holder)
- Conductive fabric strips (Iron on - may require Heat'n'Bond)
- Sewable LED light
- 3V coin cell battery
- Thread
Optional:
- Zip (for purse/wallet opening)
- Hook and Loop (hook and loop fastener) (for purse/wallet opening)
- 100% polyester or other suitable fabric for sublimation printing
- Sublimation printing paper/or iron on transfer paper alternative
Equipment required:
- Sewing machine
- Sewing needles
- Fabric scissors
- Ruler
- Fabric marker
- Iron
- Sublimation printer
Student's LED wallet/purse showing the inside LED and conductive fabric.
Student's LED wallet/purse showing the inside battery compartment and conductive fabric.
We liked the student's project as it looks great and is a lot of fun to make too. By combining electronics and circuitry with product design, e-textile manufacturing, and a bit of creativity, the student has made a solution to a simple problem that people have had for years, and ultimately a successful new product has to offer a solution...which they do in only 9 steps! If you want to have a go at making the purse/wallet yourself, you can follow his Instructables page by clicking HERE and following the simple steps. Do please send us your photos when you're finished too!
©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof without Kitronik's prior written consent.
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.
Visit TechForum