制造商零件编号 T0051388799
WSW SAC L0 SN3,0AG0,5CU3,5%
Apex Tool Group
License: See Original Project Solder
Courtesy of Kitronik
Guide by Kitronik Maker
Printed Circuit Boards (PCB) are made from layers of fibre glass and copper, glued together. Whilst the glues used are very heat resistant it is possible to overheat a PCB and damage it. Kitronik PCB designs use large tracks and pads to help make this a rare problem, the larger amount of copper helps to dissipate the heat. If a PCB is overheated the most likely outcome is that the copper layer will de-laminate from the fibre glass board. This usually leads to broken joints and a non-working circuit.
It is possible to repair some faults using adhesive copper tape and solder. Remove as little of the damage as possible to get back to a soundtrack. Cutting through the damaged tracks with a sharp knife will help to limit additional damage during removal.
Scrape a little of the solder resist off with a knife, sharp screwdriver, or fine sandpaper. Ensure that the exposed track is clean and shiny. It is also a good idea to clean any residual burnt PCB material off, to allow the tape to stick well.
Stick on some of the copper tape. Overlap the existing track very slightly.
Carefully solder the joint(s) where the repair has taken place. Most copper tape adhesive melts at soldering temperatures, so be quick and use as little heat as possible. When the tape cools the adhesive will usually remain sticky.
Rub over the pad area with a hard, rounded item, such as the none writing end of a Biro. This will push the copper tape down over the pad area. The pad hole will show through the tape, and can then be pierced with a component lead, paperclip, or similar.
The component can then be fitted and soldered in the normal manner. Keep the heat input form the soldering as brief as possible, as the adhesive and the additional joint attaching the new pad are sensitive.
The Copper tape can be cut to size with scissors, craft knife etc. Once a repair has been made it is also possible to trim the excess tape. If this is done exercise caution, as the repair is more fragile than the original PCB track and may become unstuck again.
Lesson No#. Lesson Name. Description.
Introduction. If you're new to soldering our Soldering School will have you up and running in no time.
©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof without Kitronik’s prior written consent.
Kitronik's suggested additional learning
Understanding Component Uses & Symbols
Learn about resistors, capacitors, diodes & transistors. In this guide find out what they do, how they work and what the circuit symbol is to represent them.