制造商零件编号 3860
LED ENG RED LINEAR STRIP
Adafruit Industries LLC
License: See Original Project
Courtesy of Kitronik
By Kitronik Maker
Electrician’s Guide to using the wall mount 12V 5A power supply with LED strips
Overview
This is a guide aimed at people who have experience working with mains electricity and are aware of the safety precautions that must be taken when working with high voltage electricity. It describes how to use the wall mount power supply to power up to 10M of LED strips.
DO NOT ATTEMPT TO WIRE ANYTHING INTO THE MAINS IF YOU ARE NOT QUALIFIED – SERIOUS INJURY MAY OCCUR.
You will need:
Step 1
Identify the (brown) live and (blue) neutral wires on the AC side of the terminal. These can be connected directly to a light fitting or into a plug if you prefer.
Step 2
You can connect the plug on the DC end into a 2.1mm 5A rated DC socket, as these are far more expensive than the low current version, we recommend cutting the 2.1mm plug off and running the two wires into a 2-way terminal block.
Step 3
Connect the positive and negative terminals on your terminal block to the corresponding positive and negative pads on the LED strip. If you are using a full strip then wires will already be attached to one end so you can wire these straight into your terminal, noting the polarity indicators where the wires enter the LED strip. The pads are labelled with + and – signs as can be seen in the image above.
Connecting LED strips in parallel
If you wish to use multiple LED strips exceeding a total length of 5M you must connect them to your power supply in parallel as shown in the diagram below.
Notes
A printable PDF of this guide can be downloaded here. Learn more about the author read more »
©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof without Kitronik's prior written consent.