![scheme-it logo](/zh/schemeit/img/scheme_it_logo.png?v=v1.8.7)
The RedBoard can be programmed over a USB Mini-B cable using the Arduino IDE, by selecting "Arduino UNO" from the board drop down list. RedBoard has all of the hardware peripherals which 14 digital I/O pins, 6 PWM pins, 6 analog Inputs, UART, SPI and external interrupts. The RedBoard features also I2C communication. and IOREF pins that showed up on the UNO R3, so the RedBoard will be compatible with future shields. This version adds an SMD ISP header for use with shields.
请在下方框中输入 'DELETE'(无引号),以确认进行删除操作。