A general LVDS interface is shown in the circuit in which IDT offers a full line of LVDS compliant devices with two types of output structures: current source and voltage source. The standard termination schematic as shown in the circuit can be used with either type of output structure. The LVDS interface has many applications, it is used in computer buses, screen resolutions and color depths for TV's displays panel, video interfaces for camera link standard, and other related applications.
请在下方框中输入 'DELETE'(无引号),以确认进行删除操作。