8-15 Watts DC/DC Converters for Medical and Telecom Markets
RECOM Power
This tutorial will identify new applications for DC/DC converters in the 8 to 15 W power range, beginning with a review of the existing DC/DC converter limitations and the improvements in the new RECOM families of DC/DC converters for 8 to 15 W. Also, there will be an overview of their use in those new markets or applications. Finally a list of the related RECOM DC/DC controllers available at DigiKey will be presented.
PTM Published on: 2011-03-24