Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Slide 65 Slide 66 Slide 67 Product List
LPC29xx Microcontrollers Slide 63
There are 2 power modes of operation: normal and idle mode. The device operates in normal-power mode after reset. In this mode the device is fully functional, i.e. all clock domains are available and can be enabled. In normal mode, the LPC2939 consumes typically around 1.1 mA/MHz. When the clocks are switched off, it consumes around 30 µA. The system can be put into idle-power mode either partially or fully. In idle mode, selected clock domains can be switched off using the Power Management Unit, and might also suspend execution of the software. The clock domains are enabled again upon a wake-up event. This wake-up event is provided by the Event Router. The clock domains that can be switched off during idle-power mode depend on the selected wake-up events. For an external interrupt (e.g. EXTINT0), no active clock is required, i.e. all clock domains can be switched off. However, for wake-up on a timer interrupt, the clock domain of the timer should stay enabled during low-power mode. In general, each subsystem that might cause a wake-up upon an interrupt must be excluded from the low power mode.
PTM Published on: 2011-11-02