Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Slide 65 Slide 66 Slide 67 Product List
LPC29xx Microcontrollers Slide 17
Now the presentation will focus on the Clock Generation Units (CGU), Reset Generation Unit (RGU) and the Power Management Unit (PMU). There are two clock generation units in the LPC2900 family, the CGU0, and the CGU1, both functionally identical. CGU0 is the most important unit that provides clocks to all the subsystems while CGU1 provides a clock output for all devices and provides the USB clock to devices that have a USB interface. CGU1’s input clocks are derived from CGU0.
PTM Published on: 2011-11-02