Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Slide 28
Slide 29
Slide 30
Slide 31
Product List
Thermal de-rating curves provide immediate input to the current capability of the module, based on airflow and ambient temperature. They are provided at increments of output voltage. In this example, the 12 A DLynx is selected at 1.2 V output. Next, determine the environmental conditions. In this case, it is an ambient temperature of 85ºC and natural convection (or no forced airflow). Starting from the ambient temperature and up to the natural convection curve, the operating condition point is determined. Following this operating point to the left axis, it can be seen that the module would de-rate to 11.2 A at 85ºC and no forced air. Using the same curves, it can be seen that the 12 A DLynx offers full load at 80ºC and natural convection.
PTM Published on: 2012-07-02