Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Product List
These four characters shown here represent the resistance value of the model. If the resistance is equal to or greater than 100 ohms, the first three numbers are the significant digits of the value and the fourth indicates the number of zeros that follow. Thus, 1000 would indicate a 100 ohm model.