Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
IO-Connector-Slide7

The term pin/socket refers to the mating side of the connector. In a two part connector system, the round or square profile pin in the male or plug connector wipes against a formed metal contact in the socket connector, completing a circuit. Most socket contacts are single wipe, meaning they make contact on one side of the pin. For high reliability applications, dual wipe contacts may be available.

PTM Published on: 2011-10-13