The design used on-chip One Time Programmable (OTP) memory from the PF family devices, MMPF0100NPEP as an example. It utilizes the chip which is connected to the interface tool that is used in customizing the stored program or data of the said chip. The module has different ports that enables external components to be connected with the board and would perform the necessary functions. KITPF0100SKTEVBE uses a 2x4 port compatible to flat ribbon cable (8-conductor) as interface to external components.
KITPF0100SKTEVBE is useful interface in a wide variation of configuring microcontrollers such as the OTP and others. This can be used in tablets, IPTV, eReaders, Set Top Boxes, Industrial control, medical monitoring, home automation, alarm system, energy management and other more.
Please type 'DELETE' (without quotes) to the below box to confirm the deletion: