The design is comprised of a linear actuator that drives the C-slot cylinder. The C-slot cylinder also drives the valve that controls the flow of liquid or gas. Beside the cylinder, a magnetic sensor is attached that act as a detector whether the valve is close or open. The signal produced by the sensor is transmitted to the Electronic Control Unit (ECU) using an M8 connector. The signal is processed by the ECU and transmits it to the main controller in which it provides data to the end user. The end user will provide a command that will be transmitted again to the ECU and the ECU will provide a signal that again drives the linear actuator to control the flow.
This control system design is common to industrial plants, which provides convenience to operators. However, this control system is not limited to industrial applications, it is also useful to residential applications. It can be used to control the gate, door, and window of our houses. The design is flexible since it has secure connections to its components.
Please type 'DELETE' (without quotes) to the below box to confirm the deletion: